Technical Forum

SIMATIC S7-1200

s7-1200 +PLCSIM problem

Thread Starter: kulmx   Started: 4/27/2012 11:21 AM   Replies: 12

« Previous thread Next thread »
12» Page 1 of 2 (13 items)
  4/27/2012, 11:21 AM
Joined 1/15/2007
Last visit: 1/13/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi
Help me
mac address?

Attachment: error plcsim.pdf  (92 Downloads)

Top
  4/27/2012, 11:54 AM
Joined 2/11/2010
Last visit: 6/3/2013
Posts: 199
Rating:
Rated: Outstanding [3.22 out of 5 / rated 9 time(s)]. (9) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
what do you want to do?
As I know, the simulation of a S7-1200 isn't supported by PLCSIM.
Top
  4/27/2012, 12:10 PM
Joined 1/15/2007
Last visit: 1/13/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello
Yes///
https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=29156492&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&objid=29156492&treeLang=en
Top
  4/27/2012, 12:38 PM
Joined 8/31/2010
Last visit: 6/19/2013
Posts: 1267
Rating:
Rated: Outstanding [3.88 out of 5 / rated 106 time(s)]. (106) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
kulmx wrote:
Hi
Help me
mac address?

Hello kulmx,

When did you get this? Simulation button in STEP 7 v11 will not be active.

Like it? Rate it!
Top
  4/30/2012, 9:05 AM
Joined 11/29/2011
Last visit: 6/16/2013
Posts: 65
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Is PLCSIM  possible with S7-1200 ....In forum everyone replied that simulation is not possible for 1200. Then how?



=== Edited by soju @ 4/30/2012 9:47 AM [GMT ] ===


Top
  4/30/2012, 10:35 AM
Joined 12/1/2005
Last visit: 5/3/2013
Posts: 45
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I agree with these guys there is no simulation for S7-1200.

Richard Jupp
Top
  5/2/2012, 12:06 PM
Joined 1/15/2007
Last visit: 1/13/2013
Posts: 13
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
locked
'll wait .....
cry
Top
  5/2/2012, 3:16 PM
Joined 2/16/2011
Last visit: 5/17/2013
Posts: 222
Rating:
Rated: Excellent [4.07 out of 5 / rated 15 time(s)]. (15) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
kulmx wrote:
Hello
Yes///
https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&nodeid0=29156492&lang=en&siteid=cseus&aktprim=
0&extranet=standard&viewreg=WW&objid=29156492&treeLang=en

Hello,

OK, there is PLCSim in TIA Portal, but it only works with S300 CPU's.
S7-1200 SImulation only 2013 I think..cry

Regards

Gabriel de Oliveira
It Works? Rate It.
Top
  5/2/2012, 3:29 PM
Joined 12/1/2009
Last visit: 6/11/2013
Posts: 322
Rating:
Rated: Outstanding [3.57 out of 5 / rated 28 time(s)]. (28) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dear kulmx ,

it all depends on up to what extend you want to simulate in S7-1200.

I believe that you should be able to develop and test your logic blocks with the simulator in an S7-300 project. After you can transfer that logic or blocks into your S7-1200 project.

Unfortunate I have no idea about S7-1200 that's why maybe somebody here can assist you or correct me if I am totally wrong.

Regards.


-------------------------------------------------------------------------------------------------------
Give us your feedback and show us your respect!
We take our free time to support you with our knowledge and experience.
If this post is helpfull to you kindly click on "Rate" or "Thank".
Top
  5/2/2012, 6:34 PM
Joined 8/31/2010
Last visit: 6/19/2013
Posts: 1267
Rating:
Rated: Outstanding [3.88 out of 5 / rated 106 time(s)]. (106) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
TIBI68 wrote:

Dear kulmx ,

it all depends on up to what extend you want to simulate in S7-1200.

I believe that you should be able to develop and test your logic blocks with the simulator in an S7-300 project. After you can transfer that logic or blocks into your S7-1200 project.

Unfortunate I have no idea about S7-1200 that's why maybe somebody here can assist you or correct me if I am totally wrong.

Regards.



Hello TIBI68,
It may not work out all the time as few blocks are exclusive for S7-1200 which are not supported in S7-300 like CALCULATE Instruction, some of the Math Instructions with more than two inputs (ADD, MUL), MOVE Instruction with multiple outputs etc.
And also few S7-300 blocks may not be suitable for S7-300 like S5 timer, S5 counter, etc (otherwise we would have got a simulator for S7-1200 by now - if it is similar to S7-300). This is my opinion.

Like it? Rate it!
Top
12» Page 1 of 2 (13 items)
Actions