I have measuring input set up under an axes and have P0488 setup for the input on the sinamics side. I had no issue with the measuring input until I upgraded my firmware from 4.0 to 4.1
Now I when i try to enable the measuring input i get this error:
40007 Measuring job was aborted or affected by an external device (reason: 1)
along with
30002 Command aborted (reason: 49, command type: 1403)
I can't seem to find anything wrong.
EDIT**
I was on message frame 390 before i put up the post. Then realized I needed to switch to 391. I have done so but I still am getting the same error when trying to enable the measuring input.
=== Edited by SebOber @ 4/24/2012 9:00 PM [GMT ] ===
|
-Seb