Thread Starter: Stefan_Norway Started: 4/24/2012 1:10 PM Replies: 5
I want to integrate an winCC project into Simatic.But I do not get the option in the menu for Simatic to do that.I use WinCC V7.0.0 and Simatic V5.5Could it be compability issues with these versions?Has it anything to say in witch order these are installed? WinCC was installed first.I`ve installed all the options from the instalation CD`s. And I`ve tried to install hotfix versions but this does not work with the WinCC version.BRStefan
The problem is that I do not get up the menu for OS import or WinCC, in Simatic manager.I have installed the device drivers.The example you refere to is Simatic V 5.4, it looks different in V 5.5Any other ideas?