Technical Forum

STEP 7 / STEP 7 Lite

Simple straight forward project for beginners STEP7+WinCC

Thread Starter: sky59   Started: 4/17/2012 2:20 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  4/17/2012, 2:20 PM
Joined 4/1/2012
Last visit: 9/14/2012
Posts: 30
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Though I am also beginner I finally managed after a lot of fighting to create simple and straight forward project that everyone woul understand.

So I want to share my experience with other beginners...

Project can be downloaded over here, just follow middle section without registering, only rewrite some strange characters....

http://uloz.to/xUy7idX/pidregulator-demo-wincc-rar


The project is running on SINGLE computer, it consists of:

- library PID regulator excited with either 100 or 20 value on its input, command arrives from WinCC application pushbutton, it is called every one second in OB32

- start PLCSIM with TCP/IP protocol a download software to it from simatic manager

- start WinCC project (zzz) , by pressing pushbutton you can see different required value and response from PID regulator

This design is completely minimalistic so very simple to understand!

I believe it is always better to go step-by-step not to read 1000 pages manuals..... :-)
Top
Thank you for this post from:
  4/21/2012, 1:14 PM
Joined 8/18/2009
Last visit: 4/17/2013
Posts: 464
Rating:
Rated: Outstanding [3.63 out of 5 / rated 32 time(s)]. (32) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
thanks  sky59  ...
Please tell me sample  PLC +wincc project for Redundant CPU, I/O .....so that I can understand....



=== Edited by RAJKIRAN @ 4/21/2012 1:15 PM [GMT ] ===



Rajkiran Patil

Executive Project Eng r.- Process Automation


Top
  4/21/2012, 2:49 PM
Joined 1/28/2009
Last visit: 5/20/2013
Posts: 2859
Rating:
Rated: Excellent [4.1 out of 5 / rated 394 time(s)]. (394) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
RAJKIRAN wrote:
thanks  sky59  ...
Please tell me sample  PLC +wincc project for Redundant CPU, I/O .....so that I can understand....


Hello  friends,

What is your idea to upload a Compressor simulating
module (STEP7+WINCC) applications and give this
title(see the attachment)Rnf:lblSmileyTooltip_

"Why my compressor tripped because of Surge?"

Best regards,
Hamid Hosseini

Attachment: normal_run_flow_test[17-13-50].JPG  (40 Downloads)

Human beings are members of a whole , In creation of one essence and soul
Sa'adi



Top
Page 1 of 1 (3 items)
Actions