Technical Forum

STEP 7 Additional Software

PC Adaptor USB is not detecting in ET200s

Thread Starter: shijukoshy   Started: 4/18/2012 9:42 AM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  4/18/2012, 9:42 AM
Joined 7/31/2009
Last visit: 5/1/2013
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

hello,

I'm using PC USB Adaptor ( 6ES7 972-0CB20-0XA0 ) for connecting my PG with the MPI/Profibus network.But when i coonecting the adaptor to the IM 151 (6ES7151-1AA05-0AB0)  through profibus PG connector to access the network,the adaptor doesnot show any power indications.When i refer (attached) the siemens documents it is written that it is possible to use second generation adaptors in profibus networks through ET200s.Anyone have any idea why my adaptor is not working on ET200s.


shiju


Attachment: USB MPI.pdf  (41 Downloads)

regards,
Shiju P.Koshy
+91 9971985128

Top
  4/18/2012, 10:25 AM
Joined 4/22/2010
Last visit: 5/25/2013
Posts: 3216
Rating:
Rated: Excellent [4.11 out of 5 / rated 295 time(s)]. (295) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Your Adapter needs 24V from connected CPU (through MPI cable) if not available on device or if profibus cable is used you need external power supply.

See manual for more details.

Regards,

Marcjan

Problem solved?
Please let us know!

Please no technical questions by PM, use the forum!
Top
  4/18/2012, 11:49 AM
Joined 1/3/2006
Last visit: 5/7/2013
Posts: 545
Rating:
Rated: Outstanding [3.83 out of 5 / rated 29 time(s)]. (29) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Dear,
Only ET200S CPU (IM151-7) supports this PC adapter and not IM 151.
In other words:
IM151-7 has the necessary 24V in the MPI/DP port to power a PC adapter but IM 151-1 does not !


Top
Thank you for this post from:
  4/19/2012, 9:22 AM
Joined 1/3/2006
Last visit: 5/7/2013
Posts: 545
Rating:
Rated: Outstanding [3.83 out of 5 / rated 29 time(s)]. (29) 
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
Hi,
To operate the PC Adapter USB to MPI/DP interfaces which do not have a 24V 
supply voltage, you can order an external power supply (order number: 6ES7 972-0CA00-0XA0). 
Manual of 6ES7 972-0CA00-0XA0 attached.

Attachment: 6ES7 972-0CA00-0XA0.pdf  (62 Downloads)

Top
Thank you for this post from:
Page 1 of 1 (4 items)
Actions