Technical Forum

Decentral Peripherie

Communicating to ET200Pro FC behind IM154-8F CPU

Thread Starter: rumblefish   Started: 4/16/2012 10:40 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  4/16/2012, 10:40 PM
Joined 4/16/2012
Last visit: 4/17/2012
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I'm currently working with an ET200Pro application. The setup consists of two racks on a PROFINET bus; a master IM154-8F PN/DP, and a slave IM154-4PN. Each has an ET200 Pro FC located after a F-Switch in the rack. Using STARTER i can communicate to the slave rack FC and configure the drive. The problem is trying to connect the FC located in the master rack behind the IM 154-8F. Simply put, I can't. I setup up the comms in the same manner but no luck. Are there any special considerations for the FC behind the F CPU? Can the FCPU allow pass through on the bus to see the FC? I'm at a complete loss here and would appreciate any input.

Regards
Top
  4/19/2012, 12:02 PM
Joined 2/14/2008
Last visit: 6/3/2013
Posts: 540
Rating:
Rated: Excellent [4.48 out of 5 / rated 60 time(s)]. (60) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
        See attached doc. I am also working on similar configuration.

Reagrds
 

Attachment: ET200s_FU_Safety_functions.zip  (12 Downloads)

Top
  4/19/2012, 2:35 PM
Joined 4/1/2010
Last visit: 5/16/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks for the info. The problem I'm having is that Starter will not connect to the drive residing on the same rack as the 154-8F.
Top
  4/19/2012, 3:29 PM
Joined 4/1/2010
Last visit: 5/16/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Issue resolved. Connection to an FC residing behind a cpu is not allowed.
Top
Thank you for this post from:
Page 1 of 1 (4 items)
Actions