Technical Forum

Communication / Networks

convert the RS485 two wire to RS232

Thread Starter: Sabela   Started: 3/20/2012 12:46 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  3/20/2012, 12:46 PM
Joined 3/20/2012
Last visit: 8/23/2012
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi everyone I am using a CP341 RS232 MODBUS card and I need to convert the RS485 two wire to RS232, how can I do that?
Thanks in advance



=== Edited by O_Moderator @ 3/20/2012 12:53 PM [GMT ] ===


=== Edited by O_Moderator @ 3/20/2012 12:52 PM [GMT ] ===
new subject after splitting from modbus tcp library for cpu315pn

Top
  3/20/2012, 1:04 PM
Joined 1/17/2007
Last visit: 5/17/2013
Posts: 759
Rating:
Rated: Excellent [4.33 out of 5 / rated 141 time(s)]. (141) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
This can only be done using a hardware convertor.
These are widely available (google "RS223 RS485 convertor).
Most require some form of external power supply so making them hard to implement.
However, a few actually get their power directly from the RS232 handshake lines, and thus require no external power supply.
B+B electronics make some very good ones that I have used in the past and they are available here.

Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots.

So far, the universe is winning...
Top
  3/20/2012, 1:14 PM
Joined 3/20/2012
Last visit: 8/23/2012
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thanks a lot
Top
  3/21/2012, 7:56 AM
Joined 6/17/2011
Last visit: 5/17/2013
Posts: 1272
Rating:
Rated: Excellent [4.04 out of 5 / rated 79 time(s)]. (79) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
In case you are using a PC or laptop for your communication:
I used a USB RS484 converter to a vitual com port which also worked fine. Then you don't need external power supply.

Gruß / best regards
Rated X
Top
Page 1 of 1 (4 items)
Actions