Technical Forum

STEP 7 / STEP 7 Lite

Backup S7 5.5

Thread Starter: Mario_B   Started: 3/15/2012 9:38 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  3/15/2012, 9:38 PM
Joined 3/15/2012
Last visit: 5/24/2012
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I'm a little bit of trouble in here, I want to do a full backup of the data in an old CPU 315-2DP without memory btw it's an old model so it doesn't have MMC, It does have a port for conecting a EPROM I think? but buying it's not an option. For the backup I wish something that I could erase completly the current program from the CPU and load a test one, but with the asurance that I could reupload the backup without losing any of the info and re run it again with no flaws?

Any suggestions plase?
Top
  3/16/2012, 7:11 AM
Joined 3/21/2006
Last visit: 5/14/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
How to back up a S7 PLC program
Top
Page 1 of 1 (2 items)
Actions