Hello!
I am from Belarus, my company is oil refinery “Naftan”.
We have 5 controllers of QUADLOG (CPU CCM+ 4 Mb (QLCCM22AAN)) and 4-mation Configuration Software in an old Windows NT station connected via M-BUS.
I don't know when the PC will die but it will be soon.
We want to buy a new PC and install all the software that I have.
The problem is that I don’t know if it will work in a Windows XP or Windows 2000 system. The second question is: where I can find drivers (win200, WInXP) for my m-bus PCI card installed in my PC?
Can anybody help me?
Please, give us a piece of advice, how we can solve our problem.
Thank you.
Software versions:
ProSafe-PLC SET (4-mation) Configuration Software
Version 4.37 (Release date: 09-26-2000)
ProSafe-PLC
Version 3.33 (QUADLOG)
Control Function Blocks
Version 3.20
MODBUS Master Function Blocks
Version 3.20
MODBUS Slave Function Blocks
Version 3.20
Sequence of Events Recorder Function Blocks
Version 3.20
Sequence of Events Viewer Utility
Version 4.20
Runtime API
Version 4.37
Diagnostic Logger
Version 4.40
MBUS Driver
Version 4.40 (Release Date: 08-18-2000)
ProSafe-Suite Install On: PROSAFE
Install Directory: C:\Program Files\ProSafe
Install Date 10-5-2001 12:15:05
Content of PSINSTLG.TXT:
API Runtime 4.37 C:\Program Files\ProSafe\RTAPI
ProSafe-PLC SET 4.37 C:\Program Files\ProSafe\4-mation
ProSafe-PLC Control Modules 3.33 C:\Program Files\ProSafe\4-mation
MODBUS Slave FB Library 3.20 C:\Program Files\ProSafe\4-mation
MODBUS Master FB Library 3.20 C:\Program Files\ProSafe\4-mation
Control FB Library 3.30 C:\Program Files\ProSafe\4-mation
Sequence of Events Recorder FB Library 3.32 C:\Program Files\ProSafe\4-mation
Diagnostic Logger 4.40 C:\Program Files\ProSafe\dlogger
Seq of Events Viewer Utility 4.30 C:\Program Files\ProSafe\SOE_View
APACS+ Control Panel 4.40 C:\WINNT\System32\
Installion complete 10-5-2001 12:15:25
Update MBUS Driver