Technical Forum

DC converters SIMOREG

6RA22 DC Drive showing F17 fault

Thread Starter: snakeyes   Started: 1/12/2012 6:01 AM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  1/12/2012, 6:01 AM
Joined 1/12/2012
Last visit: 1/24/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
longwalker wrote:
Hello,
I need help I have a 6RA22 DC drive and keep giving F11 fault but the encoder is fine and I have check and clean the commutator. What else can I do to get this runing?
Thanks,

good day,

i have a quite similar problem but its different fault, 6RA22 DC Drive showing F17 fault. Manuals says that this fault is "Gear Stage Not Clear" and can occur only when using supplementary boards. But i am not using any supplementary boards. A1, A2 & A5 cards im using.



=== Edited by O_Moderator @ 1/12/2012 12:17 PM [GMT ] ===
new subject after splitting from 6RA22 DC Drive showing F11 Faults

Top
  1/12/2012, 8:22 AM
Joined 4/23/2010
Last visit: 5/24/2013
Posts: 1148
Rating:
Rated: Outstanding [3.17 out of 5 / rated 53 time(s)]. (53) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
Please check parameter value E00. It must be 0. If not, change to 0 & check. If the problem didnot solve, please attach here with drive wiring details along with parameter list.
Best luck.


DEEP.

Tell me and I will forget. Show me and I will remember. Involve me and I will understand. -Confucius
Top
  1/18/2012, 8:35 AM
Joined 1/12/2012
Last visit: 1/24/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi,

thanks for your reply i highly appreciate it

i replaced the drive with 6RA70, and its working fine now. i checked 6RA22 DC Drive parameter E00 contains F2F, i dont know how it was changed coz i know it is was 0 before. but i didnt checked the drive if the F17 fault will not show up again. another thing i notice also in P10 it display 735, where is my input voltage only 380VAC, p10 should display 380 VAC isnt? what & where would be the problem?
Top
  1/18/2012, 10:21 AM
Joined 4/23/2010
Last visit: 5/24/2013
Posts: 1148
Rating:
Rated: Outstanding [3.17 out of 5 / rated 53 time(s)]. (53) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
May be problem with RAM or with EPROM. 

Tell me and I will forget. Show me and I will remember. Involve me and I will understand. -Confucius
Top
Page 1 of 1 (4 items)
Actions