Technical Forum

SIMATIC S7-400 / S7-400H / S7-400F /FH

inc. encoder instead of abs. enc.

Thread Starter: ercanbozi   Started: 1/4/2012 7:47 PM   Replies: 0

« Previous thread Next thread »
Page 1 of 1 (1 items)
  1/4/2012, 7:47 PM
Joined 4/24/2010
Last visit: 10/23/2014
Posts: 73
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear all,
I use a flying shear which is a machine driven by dc motor cuts the iron bar in my plant. An incremental encoder is used for dc motor speed control and an absolute encoder is used for flying shears knive position. I'd like to ignore the position encoder and use only inc. encoder both speed and position control, so what kind of changes must I implement in "FM 453 parameterization tool" sotware or somewhere else in the plc program.
I also want to learn how to programmed traverse blocks. I have siemens manual about this subject but couldnt understand clearly. Does anybody have different sources of traverse programming manual.
Top
Page 1 of 1 (1 items)
Actions