Technical Forum

SIMATIC TDC, FM458, T400

i have a problem with one simadyn system, the system stop and show the "H" in all CPU modules

Thread Starter: BrunoLula   Started: 12/26/2011 5:21 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  12/26/2011, 5:21 PM
Joined 12/26/2011
Last visit: 12/26/2011
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dears
i have a problem with one simadyn system, the system stop and show the "H" in all CPU modules. The power suply stay in fault state momentarily( flash the red LED). The power suplly was change two times, but the problem remains.
Someone have a sugestion? i need help.
thanks.




=== Edited by O_Moderator @ 12/28/2011 10:46 AM [GMT ] ===
new subject after splitting from simadyn D7 power supply replacement

Top
  12/27/2011, 5:53 AM
Joined 8/25/2006
Last visit: 5/21/2013
Posts: 898
Rating:
Rated: Excellent [4.2 out of 5 / rated 85 time(s)]. (85) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
BrunoLula wrote:

Dears
i have a problem with one simadyn system, the system stop and show the "H" in all CPU modules. The power suply stay in fault state momentarily( flash the red LED). The power suplly was change two times, but the problem remains.
Someone have a sugestion? i need help.
thanks.


Hello.
H is fatal system error, CPU is in stop mode, user program is not running. You need to read diagnostic data from CPU where the 'H' is flashing. Your PC/PG must be connected directly to the CPU.
What type of Simadyn D you are using? Programmed with Struc or with CFC/D7-SYS?
In CFC you may use menu command 'CPU-Module information'.
If you use Struc, you must use hex monitor, as I know.
Top
Page 1 of 1 (2 items)
Actions