Technical Forum

SIMATIC S7-200

SIMATIC S7-300/200 y SIMATIC PANEL OP73micro

Thread Starter: zeregio123   Started: 11/18/2011 8:44 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  11/18/2011, 8:44 PM
Joined 11/18/2011
Last visit: 11/19/2011
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hola!!!!

tengo un problema para poder comunicar el cpu 224 del S7-200 con un panel de control que es el SIMATIC PANEL 0P73micro, no encuentro el protocolo de comunicacion correcto, entiendo que se comunican por medio de PROFIBUS pero agradeceria que me ayudaran especificamente con el cable armado que debe llebar para tener una buena comunicacion y el panel sea el maestro y el cpu el esclavo.

de antemano muchas gracias!.
Top
  11/18/2011, 9:06 PM
Joined 4/22/2010
Last visit: 6/19/2013
Posts: 3309
Rating:
Rated: Excellent [4.12 out of 5 / rated 300 time(s)]. (300) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Welcome at the forum.

Let me first translate your question in English:

wrote:
I have a problem to setup communication betwee a cpu 224 of the S7-200 series and  a control panel which is the SIMATIC PANEL 0P73micro, can not find the correct communication protocol, I understand that panel communicate via PROFIBUS but appreciate all help , specifically with the shielded cable which should be used to have a good communication
The panel is the master and the cpu the slave.

Many thanks in advance.



The protocol is PPI, you can use a profibus cable with standard connectors for that.
You can find all the answers in the manual, chapter 4.
Here is a link, look at the bottom of the page, its in Spanish too.

http://support.automation.siemens.com/WW/view/en/21086325


Regards,

Marcjan




=== Edited by Marcjan @ 11/19/2011 11:03 AM [GMT ] ===


=== Edited by Marcjan @ 11/18/2011 9:26 PM [GMT ] ===


=== Edited by Marcjan @ 11/18/2011 9:19 PM [GMT ] ===



Problem solved?
Please let us know!

Please no technical questions by PM, use the forum!
Top
  12/2/2011, 12:46 PM
Joined 3/21/2006
Last visit: 6/18/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

The OP 73micro can be connected to the SIMATIC S7-200 via its integrated interface; the integration into networks is possible (PPI or MPI network). In case of MPI the max. baud rate is 187.5 Kbit/s. The configuration is performed exclusively with the engineering software WinCC flexible Version 2004 SP1 or higher. To download the configuration, a PC/PPI adapter cable is required (serial transfer).

Best regards,
Hristo MIhalev
Top
Page 1 of 1 (3 items)
Actions