Technical Forum

DC converters SIMOREG

S7-400 CPUs and Simoreg DC drives

Thread Starter: kamb   Started: 10/24/2011 9:36 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  10/24/2011, 9:36 AM
Joined 1/1/2008
Last visit: 1/3/2013
Posts: 35
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
I have prepared a test station with S7-400 CPUs and Simoreg DC drives. However I receive "bus fault" and "external fault" when I try to connect to drive.
Any suggestions to solve it?
Regards



=== Edited by O_Moderator @ 10/24/2011 2:21 PM [GMT ] ===
new subject after splitting from Simoreg Profibus

Top
  10/24/2011, 9:50 AM
Joined 3/21/2006
Last visit: 5/14/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
What did you do there? Give more details.
1. Make hardware copnfiguration in Step7 including the necessary GSD file corresponding to simoreg. Download it.
2. Assign in drive the same profibus address as in hardware configuration.
3. Connect both profibus connectors in drive and CPU with terminated resistors in ON. Switch on the drive. On drive profibus card has 3 leds which should blink together if everything is OK.

Best regards,
Hristo Mihalev
Top
  10/24/2011, 12:07 PM
Joined 1/1/2008
Last visit: 1/3/2013
Posts: 35
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi 
Thanks a lot. Actually when I try to install GSD file, I receive th below message:
13:4343 An update is presently not possible. In one or 
more STEP 7 applications at least one GSE 
file or type file is being referenced.
And although I have closed all windows, except that HW Config, I can not run installation.

Top
  10/24/2011, 6:20 PM
Joined 9/27/2006
Last visit: 5/20/2013
Posts: 3932
Rating:
Rated: Excellent [4.15 out of 5 / rated 619 time(s)]. (619) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello kamb;
Once you have closed all the other Simatic windows, and you only heve the HWConfig editor open, close the existing project that is running in the editor. Then you can install the gsd file.
Hope this helps,
Daniel Chartier
Top
  10/25/2011, 7:56 AM
Joined 3/21/2006
Last visit: 5/14/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Master / Slave (SIMOVERT) communication on the DP PROFIBUS
Connection of Masterdrives to Profibus-DP.

Might helps you further out in bilding of the project.

Best regards,
Hristo MIhalev
Top
Page 1 of 1 (5 items)
Actions