Technical Forum

Low-Voltage Controls

Type of grease to be used

Thread Starter: kuttysk   Started: 8/22/2011 10:22 AM   Replies: 0

« Previous thread Next thread »
Page 1 of 1 (1 items)
  8/22/2011, 10:22 AM
Joined 6/28/2011
Last visit: 9/3/2011
Posts: 7
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi everybody,
i have a concern about the type of grease for a low voltage motor bearing. The type of grease to used is mentioned in the motor side as "DIN51825-K3P-20-Li-Soap". I have Mobil Polyrex EM & Mobil Polyrex EM103 with me. can i use anyone of these? if yes, which will be the better option? please reply. hope the kind response from all.

Thank you
Take care.
Top
Page 1 of 1 (1 items)
Actions