Technical Forum

Decentral Peripherie

s7 300 and ASCON dx manager delta 2

Thread Starter: menfarhat   Started: 7/27/2011 10:20 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/27/2011, 10:20 AM
Joined 6/10/2011
Last visit: 5/8/2013
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
 hello
I need your help, I 2 ASCON M5 regulator, a manager and a DX ASCON PLC S7 300 simens
I want to play in both variabre ASCON by the PLC on the DX attraver manager

my problem and my configuration ASCON DX manager in the PROFIBUS

if you like it, how I can configure the DX manager in the PROFIBUS network and read the temperature by plc via DX manager?
Top
  7/27/2011, 12:42 PM
Joined 3/21/2006
Last visit: 5/21/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

In order to use a profibus slave is needimng a GSD file. In Simatic Manager you should assign a Profibus address which must be the same as gataway configuration. All the settings is according to http://www.asconcorp.com/library/pdf/delta2/DX_Programming.pdf  There you should assign where will be send the temperature (which word/byte) in order Profibus Master (S7-300) to know where to read it.

Best regards,
Hristo Mihalev
Top
Page 1 of 1 (2 items)
Actions