Technical Forum

SIMATIC S7-1200

S7-1200 Profibus example with MM440 motor drive

Erstellt von bakerjw am 11.05.2011 21:28 (0 Antworten)

« Vorheriges Thema Nächstes Thema »
Seite 1 von 1 (1 Objekte)
  11.05.2011, 21:28
Beigetreten am: 14.03.2008
Letzter Besuch: 17.05.2013
Beiträge: 110
Bewertung:
Bewertung: Exzellent [4,08 von 5 / 13 mal bewertet]. (13) 
Bewertung: Exzellent [5 von 5 / 2 mal bewertet]. (2) 
The other day Pegaia posted a sample project showing motor drive control using Profinet from an S7-1200. I decided to throw together one similar in function for Profibus.

I put this small demonstration project together using TIA Portal 11 Professional using an S7-1214 to control a MicroMaster 440 drive. The motor drive is configured with 2 PZD words and 4 PKW words. It is a very basic implementation similar in function to the USS library. The GSD file is included as part of the project.

Off 2 and Off 3 need to be set true prior to setting RUN to true. The Speed_SP will accept values between +200.0 and -200.0 with the values being percent of motor speed.

There will be Profibus support with the Basic version of the TIA portal when it is released.

Dateianhang: S7-1200_MM440_Profibus_DP.zip  (1088 Downloads)



=== Edited by bakerjw @ 5/11/2011 9:31 PM [GMT ] ===



Top
Für diesen Beitrag bedankt sich:
Seite 1 von 1 (1 Objekte)
Aktionen