Contact
|
|
|
|
|
Login
|
Register
Print document
Technical Forum
STEP 7 Additional Software
PID implementation
Thread Starter:
BulentO
Started:
12/23/2006 12:01 PM
Replies:
1
« Previous thread
Next thread »
Page 1 of 1 (2 items)
12/23/2006, 12:01 PM
BulentO
Joined 7/23/2006
Last visit: 10/5/2011
Posts: 10
Rating:
(0)
(0)
Dear Sir,
May be this question was asked before but i searched this Forum but could not find any satisfying answer.
I want to control a water valve according to a tank temperature in my automation task. details are ; Tank temperature Set Point (SP) : 25 degree , allowed band width is +, - 2 degree (27-23) .my high limit is 35 degree and minimum tank temp is. 10 degree .
I want my water valve fully open %100 at 35 degree and fully closed at 10 degree.
I studied this problem but coulndt solve. in FB41 manipulated value LMN goes suddenly to 100 when temperature goes over 27. and goes suddenly to 0 when temp. below 23.
for example I want my valve to open % 70-80 when goes over 27.
How can i configure these parameters in FB41. also information i used are Gain :1 , PV_FAC :1 , LM_HLM : 100, LM_LLM : 0, TI time :20 sec, TD time 20 sec. no manuel control selected.
İ called also this block in OB1.
Please inform me as soon as possible because now the task is controlled manually.
Best Regards,
Bulent Ozigci
Top
12/23/2006, 12:44 PM
Late
Joined 1/7/2006
Last visit: 4/30/2013
Posts: 2667
Rating:
(253)
(1)
Hi B,
FB41 is a PID block and can not use certain stands for the output, you then have to built them by your self on the outside.
The blocking of the valve for certain places (min/max) is easily to do with the minimum and maximum range of the output of FB41.
With Modulaire PID you can do this very easy. Thats a package to built all kind off controllers that are not standard.
See the handbook:
Modular PID Control
and
Modular PID Control Getting Started
for more infornation and possibilitys of the modular PID blocks.
So you might use this blocks or you have to built it around FB41 (Tip: block the controller when you are on a range where you didn't want that the valve is opened further or less, because you will be get a windup of the I-action of the PID controller).
I hope that the answer will help, if you have still questions, don't hesitate to ask me.
All the best, Late
Never say never, think in solutions, not in trouble......
Top
Page 1 of 1 (2 items)
Actions
Copy Link
To conference
Product Conferences
LOGO!
SIMATIC TDC, FM458, T400
SIMATIC S7
SIMATIC S5 / STEP 5
SIMATIC 505
Communication / Networks
Programming Devices
PC-based Automation
Industrial PC SIMATIC PC
Decentral Peripherie
Industrial Software
Industrial Software general
STEP 7 (TIA Portal)
STEP 7 / STEP 7 Lite
STEP 7 Additional Software
SIMATIC Addons / IT4Industry
Process Control Systems SIMATIC PCS 7
Process Control System - APACS+
Process Control System - QUADLOG
Teleperm M / WinCC-TM / PCS 7 - TM
Other Process Control Systems
Visualization
SINUMERIK / SIMODRIVES / MASTERDRIVES / SIMOTION / SINAMICS
SINUMERIK CNC automation systems
SIMODRIVE Converter system
SIMOVERT MASTERDRIVES
Motion Control System SIMOTION
SINAMICS
MICROMASTER
ROBICON Perfect Harmony - Medium voltage converters
DC converters SIMOREG
SIMOTICS
Drive Tools
Process Instrumentation / Analytics / Weighing Systems SIWAREX
SIMATIC Ident
Low-Voltage Controls
Building Technology
General Conferences
Quick Links
All Conferences
The new Threads
Highlight Threads
Contact
Support Request
Contacts Worldwide
Moderator
Users online
leonlai909
,
Berkant
,
egroj
,
shadowman6xx
,
usb
,
Epaminondas
,
demo22
,
labirex
,
vanDyk
,
TomTom307
,
R&H CO.
,
ottogehtbaden
,
Martin Brion
,
SSanz
Help
Online Help
Guided Tour