Technical Forum

PC-based Automation

Connecting Wonderware InTouch + Soft PLC + Simulink

Thread Starter: linkorn86   Started: 2/7/2011 3:29 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  2/7/2011, 3:29 PM
Joined 2/7/2011
Last visit: 2/14/2011
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi everyone!
I'm new here, and I have some problems that I can't solve by myself...!!  

I have to do a plant simulation in a computer, connecting Wonderware Intouch with some Soft PLC through OPC, and this Soft PLC to Simulink. I'd like to know which Soft PLC is good for this connection, and how to connect them. Also I've heard there is something called PAC, that is similar to a Soft PLC, but I don't know if I can use a PAC instead of a Soft PLC, or which is better.

Which Soft PLC or PAC should I use?

Thanks! 

Top
  2/7/2011, 4:23 PM
Joined 1/22/2009
Last visit: 5/13/2013
Posts: 82
Rating:
Rated: Outstanding [3.86 out of 5 / rated 7 time(s)]. (7) 
Users with special expertise supervising conferences
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hello,

the SIMATIC WinAC RTX 2010 (F) is the realtime SoftPLC from SIEMENS: http://support.automation.siemens.com/WW/view/de/44388946

With it comes also an OPC-Server for your OPC connection. An other possibility is "WinAC ODK" for communication with an "own" application written in e.g. C/C++/C# directly with the softplc WinAC RTX.
http://support.automation.siemens.com/WW/view/de/35067305

I'm not familiar with Wonderware Intouch, but I think there are drivers for S7 connection, which is needed to connect intouch with an SIMATIC PLC controller.

regards
Top
Thank you for this post from:
  2/7/2011, 4:45 PM
Joined 2/7/2011
Last visit: 2/14/2011
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you for your fast reply!

I'll try with this software.
Top
  2/8/2011, 7:20 AM
Joined 3/21/2006
Last visit: 5/14/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

And to continue connection of this soft PLC to Intouch.togue Look there -  Intouch and PLCsim . And if you have some ideas for connection with Simolink, please share with us.

Best regards,
Hristo Mihalev
Top
  2/9/2011, 1:14 AM
Joined 2/9/2011
Last visit: 3/8/2011
Posts: 7
Rating:
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Rated: Outstanding [4 out of 5 / rated 1 time(s)]. (1) 
Simulink is supported as an OPC DA Client via MathWorks OPC Toolbox.  If I understand properly, your plant model is in Simulink and Soft PLC is your controller.  If Soft PLC has an OPC DA Server, connecting it to Simulink is straight forward via the OPC Toolbox.  The only thing to consider is the speed of the simulation.  You can set Simulink to run in "real-time" which means it is using the host computer's internal clock.  You can speed up and slow down the simulation also. The OPC-approach should be fine for most process applications.  If you are looking for something faster, such as modeling a motor drive system, the OPC-approach will likely be too slow.

Regarding InTouch, I am not familiar with this, but it appears to be an HMI.  Wonderware does have OPC connectivity so you should be able to connect this to Simulink and Soft PLC.

If you want to go into this in more depth, I can put you in touch with a local resource.



=== Edited by O_Moderator @ 2/9/2011 7:31 AM [GMT ] ===
contact data deleted

Top
Thank you for this post from:
Page 1 of 1 (5 items)
Actions