Technical Forum

Process Control System - QUADLOG

cpu-400FH specification

Thread Starter: Meisam_s   Started: 1/1/2011 1:13 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  1/1/2011, 1:13 PM
Joined 1/1/2011
Last visit: 1/8/2011
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi friends

i want to work with cpu-400FH and i had some information about it however,
more technical and specification of this in compare with QUADLOG can help me

best regards.
Top
  1/1/2011, 1:23 PM
Joined 1/28/2009
Last visit: 5/22/2013
Posts: 2863
Rating:
Rated: Excellent [4.1 out of 5 / rated 394 time(s)]. (394) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear member

please check this post for more information.

Difference between Quadlog and S7-400FH

regards

Human beings are members of a whole , In creation of one essence and soul
Sa'adi


Top
  1/3/2011, 8:54 AM
Joined 1/1/2011
Last visit: 1/8/2011
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

Dear hdhosseini
I read it before but it has not enough information about cpu-400FH it eliminate QuadLog however it has not data about CPU-400FH Please Help Me.

Thanks .

Top
  1/3/2011, 12:01 PM
Joined 1/28/2009
Last visit: 5/22/2013
Posts: 2863
Rating:
Rated: Excellent [4.1 out of 5 / rated 394 time(s)]. (394) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear member

check this link:
fail safe & fault tolerant

Well explained basic terms of H &F ,thanks dchartier
check the manuals proposed by dchartier:
dchartier schrieb:

As a very basic definition,
-a fault-tolerant system (also known as High-availability system, as in S7-400H) is designed to reduce production loss by using a pair of redundant processors in a Primary/Standby mode. Its main objective is to minimize downtime. Redundancy can be used in various configurations, and at various levels (controller, I/O, communications, cables....) depending on the required protection required.
Here you will have information on the S7-400H system, and basic information:
http://support.automation.siemens.com/WW/view/en/1186523

- a fail-safe system (Fail-safe as in S7-400F) is designed to protect human life (and injury), the environment and manufacturing investments by determining safe operating modes, and bringing the control; system to a "safe" STOP mode in case the situation is evaluated as unsafe. Again, many configurations and levels can be configured, depending on the standardized safety level required (often determined by SIL analysis).
Here you can find a manual on Safety Engineering in S7 Systems, for more information:
http://support.automation.siemens.com/WW/view/en/12490443
In Siemens' world, you can have a mixture of both concepts, as in S7-400HF systems.


Best regards

Human beings are members of a whole , In creation of one essence and soul
Sa'adi


Top
  1/8/2011, 1:36 PM
Joined 1/1/2011
Last visit: 1/8/2011
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
THANKS .

Top
Thank you for this post from:
Page 1 of 1 (5 items)
Actions