Technical Forum

MICROMASTER

Profidrive Status Word 1 Bit 9 MM440

Thread Starter: horsman   Started: 12/3/2010 1:51 AM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  12/3/2010, 1:51 AM
Joined 9/19/2006
Last visit: 5/15/2013
Posts: 27
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

What controls the status of bit 9 in Status Word 1 of the Profidrive profile in an MM440? According to what I have read, it seems to me that this bit should toggle when switching between local and remote control on the drive. In my case, this does not happen. Bit 9 is always ON.

Thanks
Top
  5/20/2011, 5:14 PM
Joined 7/8/2009
Last visit: 5/17/2013
Posts: 1167
Rating:
Rated: Excellent [4.25 out of 5 / rated 326 time(s)]. (326) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Well, in Manual it says its always 1 but I think its related to Control Word Bit 10..

Try to change this Bit and check Status of that Status bit

Devesh

Please say Thanks if your Problem is Solved.. :-)
Top
  6/1/2011, 7:43 PM
Joined 2/14/2011
Last visit: 9/14/2012
Posts: 63
Rating:
Rated: Above avarage [3 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
horsman wrote:
Hello,

What controls the status of bit 9 in Status Word 1 of the Profidrive profile in an MM440? According to what I have read, it seems to me that this bit should toggle when switching between local and remote control on the drive. In my case, this does not happen. Bit 9 is always ON.

Thanks



Hello,

Bit 9 of status word 1 is PZD control in MM440. It is always high.

It is not status of Local/Remote selection.

If you have required Local/Remote status, then send r52 to the PLC from drive.


Regards
Pranab

Attachment: Status word.GIF  (25 Downloads)

Top
Page 1 of 1 (3 items)
Actions