Technical Forum

SIMATIC WinCC

Wincc Web Navigator and Windows 7

Thread Starter: yac   Started: 8/17/2010 9:07 AM   Replies: 13

« Previous thread Next thread »
12» Page 1 of 2 (14 items)
  8/17/2010, 9:07 AM
Joined 6/17/2009
Last visit: 3/20/2013
Posts: 22
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear all,

I have wincc V6.0 SP2 and its web navigator V6.1 SP1. These versions are working properly with windows XP. I tried to connect to the wincc application through a new PC with Windows 7. The software was installed successfully (Web Navigator + Basic Process Control) but I could not connect to the server. The message "Connecting to server" keeps appearing and the internet explorer hangs.

Can any one help me in this issue? Is the web navigator not compatible with Windows 7 ?

Thanks
Top
  8/17/2010, 9:14 AM
Joined 3/5/2009
Last visit: 5/6/2013
Posts: 347
Rating:
Rated: Outstanding [3.49 out of 5 / rated 39 time(s)]. (39) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello yac,
just see this faq.
Which operating system and software do you require for the SIMATIC WinCC Web Navigator V1.x, V6.x and V7.x?

So i think Web Navigator v6.1 SP1  isn´t compatible with Windows 7.

Best regards
Bilao



=== Edited by bilao @ 8/17/2010 9:15 AM [GMT ] ===


Top
  8/17/2010, 10:18 AM
Joined 6/17/2009
Last visit: 3/20/2013
Posts: 22
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Bilao,

Thanks for your reply. I cannot understand the reason although the internet explorer version for both WinXP and Win7 is the same (version 8) and I use the Windows 7  as 32bit, the web client is not working. Is there any settings in the windows 7 that I can make in order to be similar to XP?

Best regards
Top
  11/18/2010, 6:32 PM
Joined 11/18/2010
Last visit: 1/11/2011
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi! i have the same problem. i need the solution please!!!
Top
  12/13/2011, 8:30 AM
Joined 8/18/2010
Last visit: 4/24/2013
Posts: 31
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear all,
Unsuitability between WinCC Webnavigator and Windows 7 causing  from ISS structure and version not from Internet Explorer.Please check the ISS version in both XP and Win7.



Regards.
Top
  12/13/2011, 9:50 AM
Joined 4/30/2008
Last visit: 5/20/2013
Posts: 628
Rating:
Rated: Outstanding [3.94 out of 5 / rated 36 time(s)]. (36) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I have wincc web navigator 6.2 running and i am able to see them on windows 7  pc but i had to use the client from wincc 7.0 to allow the explorer to function .

Regards


Steve

Some people are like slinkies
they are really good for nothing
but they still bring a smile to your
face when you push them down the stairs!!!
Top
  12/13/2011, 10:14 AM
Joined 10/11/2006
Last visit: 5/16/2013
Posts: 1741
Rating:
Rated: Outstanding [3.45 out of 5 / rated 77 time(s)]. (77) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

WinCC WebNavigator 6.2 is not compatible with WinCC V7.0

see FAQ

http://support.automation.siemens.com/WW/view/en/21927773
Top
  12/13/2011, 11:20 AM
Joined 4/30/2008
Last visit: 5/20/2013
Posts: 628
Rating:
Rated: Outstanding [3.94 out of 5 / rated 36 time(s)]. (36) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I am running wincc 6.2 web navigator but on the windows 7 machines i had to load the client from wincc 7 and it does work . We were running wincc 6.2 on windows 2003 server and upgraded our pc's to windows 7 , we are still running the wincc 6.2 on the 2003 server I just needed to install the wincc 7.0 client on the windows 7 machines for the internet explorer to function and have not had any problems with it as of yet and this setup has been running for about 6 months

Regards


Steve

Some people are like slinkies
they are really good for nothing
but they still bring a smile to your
face when you push them down the stairs!!!
Top
  3/12/2012, 3:22 PM
Joined 3/12/2012
Last visit: 4/21/2013
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
dear all.

I want set web navigator with windows 7 too. how set this web navigator with windows 7?
I installed all plugin, but hees don't work. 
'Connecting to Server...' and hung.
Someone already configured it? Please help in this problem!!!

sorry for broken English.  
Top
  8/2/2012, 9:16 AM
Joined 4/18/2011
Last visit: 3/15/2013
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

did you solved the problem, because I also have this problem?
Top
12» Page 1 of 2 (14 items)
Actions