SIMATIC Addons / IT4Industry
SIMIT -> PLCSIM -> program in SIMATIC COMMUNICATION PROBLEMS
Thread Starter: fikos Started: 5/31/2010 11:29 AM Replies: 0

5/31/2010, 11:29 AM
|
Joined 5/15/2010
Last visit: 9/21/2010
Posts: 7
Rating:
(0)
|
(0)
|
Hi there Im using SIMATIC V5.3 + HF2, PLCSIM V5.3, SIMIT SCE V5.0 SP1
I have the communication problem.
I have done it like it is in manual. I created a PLCSIM getaway in Simit and after I download the program into the PLCSIM and start simulation its not working at all. When Im not doing download I can change the outputs in PLCSIM and see it in Simit, and can change inputs in Simit and see it in PLCSIM. Unfortunatelly I need to communicate Simit with the written program, as the program changes the outputs.
Any help aprreciated.
Regards Bart
|
|
|
|
Actions