SIMATIC ProTool / ProTool/Pro
ProTool; MP370 Boot-Sequence
Thread Starter: Import-User-1 Started: 9/5/2005 2:23 PM Replies: 1

9/5/2005, 2:23 PM
|
Joined 8/10/2005
Last visit: 5/15/2013
Posts: 3031
Rating:
(17)
|
(0)
|
Hello,
we use the MP370. If have the effect, that the panel doesn´t start correct sometimes. This happend when I switch power on in the morning or after loading the project from the engineering-PG to the panel. Normaly I use seriell-download. Using MPI/Prfibus I havn´t seen the problem till now. The system is booting normaly, than the first project-screen is opening and than: "Nothing!" The screen is froozen. The data from the PLC are not received, there is no touch- or key-use possible. Only power-OFF and ON make the system usable. We use ProTool V6.0SP2. Not ProToolPro! The panels are the last generation. Happend with 12" Touch, 15"Touch and 15" Key. Using CPU414-3DP wia DP, CPU313C via MPI It doesn´t seems to be a transfer-problem, because after power-OFF/ON the panel works well. Also it can´t be a timing-problem about PLC and panel. It happens when PLC is running and only loading the panel. With best regards
Frank
|
|
|
|

9/5/2005, 2:23 PM
|
Joined 8/10/2005
Last visit: 12/13/2012
Posts: 1471
Rating:
(21)
|
(0)
|
|
|
|
|
Actions