Technical Forum

SIMATIC 505

TI-505 Communication to S7-416 3dp

Thread Starter: Begginer   Started: 11/8/2009 6:36 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  11/8/2009, 6:36 PM
Joined 5/13/2008
Last visit: 11/22/2009
Posts: 42
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Colleagues,

Good evening I just want to ask if someone knows a way to send and recieve data from s7-400 to TI-505 CPU. Thank you very much in advance.

Warm regards,
Begginer
Top
  11/8/2009, 9:00 PM
Joined 9/27/2006
Last visit: 11/24/2009
Posts: 1325
Rating:
Rated: Outstanding [3.91 out of 5 / rated 219 time(s)]. (219) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Beginner;
The foolowing FAQ will show you different ways you can interface between a TI505 and a S7 CPU:
http://support.automation.siemens.com/WW/view/en/5854042

The different selections are material-dependant, that is your choice is limited by the hardware you have in the various CPUs. The availability of communications modules will be especially critical on the TI505 side, as Siemens does not produce them any more -- look at the CTI site for alternatives, if required (http://www.controltechnology.com/).
The easiest way to send 244 bytes In and OUT between the CPUs would be Profibus-DP (generally available on both CPUs); you can either set the S7 as a slave on the bus and use COM Profibus to coonfigure the exchanges on the TI505 side; or you can use a DP/DP coupler, which acts as a slave to both CPUs (acting as master).
For any more details at this stage, start by skimming the available manuals on the suggested FAQ, and come back here for more help.
Hope this helps,
Daniel Chartier



=== Edited by dchartier @ 11/8/2009 9:38 PM [GMT ] ===


Top
Thank you for this post from:
  11/20/2009, 6:57 PM
Joined 5/13/2008
Last visit: 11/22/2009
Posts: 42
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you very much Daniel, by the way is it possible to use two dpdp coupler just in case i need to connect my s7 cpu to 2 TI-505 cpu. Thank you very much

I believe this is possible if my s7-cpu have at least 2dp port. Please confirm this. Thank you very much...



=== Edited by Begginer @ 11/20/2009 7:07 PM [GMT ] ===


Top
  11/21/2009, 12:24 AM
Joined 9/27/2006
Last visit: 11/24/2009
Posts: 1325
Rating:
Rated: Outstanding [3.91 out of 5 / rated 219 time(s)]. (219) 
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hello Begginer;
Yes, you may use a DP/DP coupler on any DP master port. Actually, you are not limited to a single DP/DP coupler per bus, it is considered a single ordinary slave on each configurator.
Hope this helps,
Daniel Chartier
Top
Thank you for this post from:
Page 1 of 1 (4 items)
Actions