SIMATIC S7-200
plc simatic s7 200 and power supply
Thread Starter: sotos Started: 9/24/2009 6:04 PM Replies: 1

9/24/2009, 6:04 PM
|
Joined 6/5/2009
Last visit: 1/5/2012
Posts: 12
Rating:
(0)
|
(0)
|
Hi all! I have a simatic s7-200 with cpu 6ES7 212-1BA01-0XB0 but i don't know with which power supply to connect it. Should i connect it with the 230VAC at home? The manual says:
Voltage/frequency range 85 to 264 VAC at 47 to 63 Hz Input current 4 VA typical, CPU only 50 VA maximum load Holdup time 20 ms minimum from 110 VAC Inrush current 20 A peak at 264 VAC Fusing (non-replaceable) 2 A, 250 V, slow blow 5 VDC current 260 mA for CPU 340 mA for expansion I/O Isolated Yes. Transformer, 1500 VAC, 1 min
Best regards, Sotos
|
|
|
|

9/25/2009, 1:32 AM
|
Joined 5/4/2009
Last visit: 5/20/2013
Posts: 697
Rating:
(22)
|
(0)
|
Dear Sotos...
With the specification you mentioned, you can supply the CPU from the power supply plug at your home yes, but be careful that the power supply at your home meets the specification you mentioned.
Have luck. Tomy the Master.
Aim Higher
|
|
|
|
Actions