Technical Forum

Process Control System - QUADLOG

Raw value for a Analog Channel

Thread Starter: S K Rewliya   Started: 9/21/2009 9:35 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  9/21/2009, 9:35 PM
Joined 12/27/2007
Last visit: 1/27/2012
Posts: 13
Rating:
Rated: Very Good [2 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi
New to Quadlog system,please tell me how to see the raw value (mA of the Input)of an analog Input in a CAM card.I m using 4-mation 4.52 MBUS.
It`s quite easy in S7,but here I have no idea.
Thanks in advance.
Regards,
SKR



=== Edited by S K Rewliya @ 9/21/2009 9:37 PM [GMT ] ===


Top
  9/29/2009, 4:21 PM
Joined 12/20/2005
Last visit: 4/23/2013
Posts: 78
Rating:
Rated: Excellent [5 out of 5 / rated 3 time(s)]. (3) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello SKR,

Unfortunately QUADLOG does not support displaying the raw data value. You could convert the conditioned signal back to mA using a SCALER function block by configuring the engineering in low (EINL) and high (EINH) softlist parameters of the FB to your engineering range (0 - 100% for ex.) and the engineering outs (EOUTL and EOUTH) to 4 and 20 respectively.

Best regards,
RJP
Top
Page 1 of 1 (2 items)
Actions