Technical Forum

SIMATIC S7

Difference in S7 300 and S7 400

Erstellt von mohit am 08.07.2009 21:30 (18 Antworten)

« Vorheriges Thema Nächstes Thema »
12» Seite 1 von 2 (19 Objekte)
  08.07.2009, 21:30
Beigetreten am: 25.02.2009
Letzter Besuch: 18.09.2011
Beiträge: 90
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
What is the deffrence between Siemens S7-300 & S7-400 PLC?
Top
  09.07.2009, 04:25
Beigetreten am: 20.12.2008
Letzter Besuch: 24.05.2013
Beiträge: 473
Bewertung:
Bewertung: Herausragend [3,37 von 5 / 209 mal bewertet]. (209) 
Bewertung: Sehr gut [2 von 5 / 2 mal bewertet]. (2) 
Hi Mohit,

There might be different views for looking at the differences. 

However in Layman's Language S7-400 Systems are made for bigger complex and large machinery system where number of I/O's are higher and having much advanced features. Probably there will be a long list due to different parameters one will be looking at.

I can give you an anlogy which probably makes you much more clear, Like the difference in Maruti-800 and Maruti-Zen.

If you would have any question about particular S7 300 Module and 400 module then it would be easy to explain.

Top
  09.07.2009, 06:05
Beigetreten am: 09.11.2005
Letzter Besuch: 22.05.2013
Beiträge: 444
Bewertung:
Bewertung: Herausragend [3,77 von 5 / 22 mal bewertet]. (22) 
Bewertung: Exzellent [5 von 5 / 2 mal bewertet]. (2) 
lalit wrote:
Hi Mohit,

I can give you an anlogy which probably makes you much more clear, Like the difference in Maruti-800 and Maruti-Zen.


You learn something everyday , didn't know Maruti was a car.This side of the world I would compare a VW golf and an Audi quatro

Below is a reply to a similar tread , stolen from Daniel .I hope he doesn't mind but I could not explain it better than this
Hello;
Siemens rates the S7-300 as a medium level PLC, and the S7-400 as a high-level PLC. So there are differences in work memory, processor speed, number of communication links and I/O connectivity.
First point, the S7-400 family is rack-based (Multi-pin backplane linking all modules, from power supply to I/Os) whereas the S7-300 is a bus-linked platform (a serial connector links all modules). So essentially the physical layout limits the S7-300 back[plane exchanges to MPI speeds (187,5 Bits per second), whereas the S7-400 uses parallel connections over the backplane rack, permitting higher exchange rates, and a higher module-density.
Second point, the form factor of the S7-300 is smaller, more compact than the S7-400, so this is something to take into account if space is a premium (inside a small machine panel, for example).
Now, the higher S7-300 CPUs (especiatlly for the new S7-317 and S7-319)have specs that approach (and sometimes pass) the specs of lower end S7-400 CPUs, so the distinction is starting to blur.

Hope this helps,
Daniel Chartier


Greetings

Eric



=== Edited by aikona @ 7/9/2009 6:05 AM [GMT ] ===



Here we only work on 'no need to know basis' ,just fix whatever is wrong
Top
  10.07.2009, 04:23
Beigetreten am: 25.02.2009
Letzter Besuch: 18.09.2011
Beiträge: 90
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Thanks aikona very gud and clear explaination of the difference
Top
  10.07.2009, 04:24
Beigetreten am: 25.02.2009
Letzter Besuch: 18.09.2011
Beiträge: 90
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Thanks lalit
Top
  02.09.2009, 22:54
Beigetreten am: 07.12.2008
Letzter Besuch: 02.09.2009
Beiträge: 2
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
The S7 400 is capable of "hot redundancy".  In case of the master PLC failure, the secondary PLC can take over without missing a step.
Top
  05.10.2009, 15:45
Beigetreten am: 05.10.2009
Letzter Besuch: 23.10.2009
Beiträge: 2
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Hi everybody,

Yours answers are really interesting, but I need more details. Is there any difference about communication management between S7-300 and S7-400?

Thanks by advance.

Best Regards,



=== Edited by jtoussaint @ 10/5/2009 3:46 PM [GMT ] ===


Top
  05.10.2009, 17:04
Beigetreten am: 25.02.2009
Letzter Besuch: 18.09.2011
Beiträge: 90
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Please go through the answer by aikona.
Top
  05.10.2009, 17:07
Beigetreten am: 25.02.2009
Letzter Besuch: 18.09.2011
Beiträge: 90
Bewertung:
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
What is the difference in the CPU-315 and CPU-317.
Top
  05.10.2009, 18:02
Beigetreten am: 31.08.2005
Letzter Besuch: 24.05.2013
Beiträge: 984
Bewertung:
Bewertung: Herausragend [3,85 von 5 / 122 mal bewertet]. (122) 
Benutzer mit speziellen Fachkenntnissen, die einzelne Konferenzen betreuen
Bewertung: keine [0 von 5 / 0 mal bewertet]. (0) 
mohit wrote:
What is the difference in the CPU-315 and CPU-317.

mainly performance, memory size and, of cause, the price.

e.g. calculating time, max size of FB, max number of FB.

mfG / Best Regards

Dirk
Top
12» Seite 1 von 2 (19 Objekte)
Aktionen