Technical Forum

SIMATIC TDC, FM458, T400

FM458 cannot restart

Thread Starter: cohiba   Started: 12/12/2008 1:18 PM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  12/12/2008, 1:18 PM
Joined 12/12/2008
Last visit: 12/27/2010
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

after hardware config ,download to 458, but 458 cannot start to run. the yellow lamp of stop is always light. I hope to know the way to let it run. thank you!

the information of diagnostic buffer:

Diagnostic buffer of module 4581DP

Order No./ Description         Component                      Version                      
6DD1607-0AA1                   Hardware                       6                            
- - -                          Firmware                       V 1.1.4                      

Rack:                          0
Slot:                          5


Event 1 of 100:  Event ID 16# 430E
Memory reset executed
Previous operating mode: STOP (memory reset)
Requested operating mode: STOP (own initialization)
Incoming event
11:49:33.655 AM  12/09/2008


Event 2 of 100:  Event ID 16# 4309
Memory reset started automatically (power on not backed up )
No relevance for user (Z1): 0300
Previous operating mode: No voltage
Requested operating mode: STOP (memory reset)
Incoming event
11:49:31.145 AM  12/09/2008


Event 3 of 100:  Event ID 16# 494E
Power failure
Previous operating mode: STOP (internal)
Requested operating mode: No voltage
External error, Incoming event
11:49:29.644 AM  12/09/2008

Top
  12/12/2008, 4:51 PM
Joined 8/31/2005
Last visit: 6/19/2013
Posts: 997
Rating:
Rated: Outstanding [3.85 out of 5 / rated 122 time(s)]. (122) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
there must be another LED light on the FM458. Which one?
Do you have a MMC in the FM (I think yes, because you wrote you made the download)
The FM458 only runs up when the S7-CPU runs up.

mfG / Best Regards

Dirk
Top
  12/13/2008, 1:36 AM
Joined 12/12/2008
Last visit: 12/27/2010
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
thanks miami.

no others lamp are light.only stop lamp of 458 is light.

I have MMC card 2MB

there are  CPU416 along with FM458 on the same rack
Top
  12/16/2008, 6:20 PM
Joined 8/31/2005
Last visit: 6/19/2013
Posts: 997
Rating:
Rated: Outstanding [3.85 out of 5 / rated 122 time(s)]. (122) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Can you test the MMC with a S7-300 CPU? Is the CPU in RUN?

mfG / Best Regards

Dirk
Top
  12/17/2008, 2:35 PM
Joined 12/12/2008
Last visit: 12/27/2010
Posts: 4
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
thanks miami!
Top
Page 1 of 1 (5 items)
Actions