Technical Forum

Process Control Systems SIMATIC PCS 7

PCS7 and PCS7 Batch , Holding Recipe on error

Thread Starter: CAG168   Started: 8/3/2012 9:29 PM   Replies: 0

« Previous thread Next thread »
Page 1 of 1 (1 items)
  8/3/2012, 9:29 PM
Joined 12/13/2006
Last visit: 8/5/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear All,

     In my CFC chart for the SFC type I have connected the Hold input of the SFC to a process error to stop a phase in my batch.
     But is there any way of stopping the whole running recipe as well as only the phase.

     Ihave try the CmdPropagation and the TriggerCmdPropagation.  But it only stop the Held phase and the Unit on the Top of the Recipe but not any phases inbetween ?????  (I had a continuous phase in between).  If I use the Hold from the BCC that everything will hold.



=== Edited by CAG168 @ 8/3/2012 9:30 PM [GMT ] ===


=== Edited by CAG168 @ 8/3/2012 9:30 PM [GMT ] ===


Top
Page 1 of 1 (1 items)
Actions