Technical Forum

SIMATIC WinCC flexible

wincc flex 2008 installation

Thread Starter: Algudkar   Started: 7/2/2012 7:46 AM   Replies: 13

« Previous thread Next thread »
12» Page 1 of 2 (14 items)
  7/2/2012, 7:46 AM
Joined 7/25/2009
Last visit: 5/23/2013
Posts: 409
Rating:
Rated: Very Good [1.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi experts and friends
now in my pc having windows 7xp os
iam going to install wincc flexible 2008 but it giving the error which following pop dialog

  "The following program could not be installed.
  microsoft SQL server2005 Express edition set up cannot complete the installation
  -1"
 can any body help me

regards
Algudkar sh..

Top
  7/2/2012, 8:14 AM
Joined 9/28/2005
Last visit: 5/21/2013
Posts: 2912
Rating:
Rated: Excellent [4.02 out of 5 / rated 208 time(s)]. (208) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
algudkar wrote:
Hi experts and friends
now in my pc having windows 7xp os
iam going to install wincc flexible 2008 but it giving the error which following pop dialog

  "The following program could not be installed.
  microsoft SQL server2005 Express edition set up cannot complete the installation
  -1"
 can any body help me


First of all, there is not operating system Windows 7XP. Other thing, we need more info. Is it fresh install ? Maybe you have other version of SQL installed ? What other software do you have in your PC ? Also you can read this What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?

Regards,
--------------------------------
Darius
Automation engineer/programmer
Top
  7/2/2012, 3:27 PM
Joined 7/25/2009
Last visit: 5/23/2013
Posts: 409
Rating:
Rated: Very Good [1.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Darius wrote:
algudkar wrote:
Hi experts and friends
now in my pc having windows 7xp os
iam going to install wincc flexible 2008 but it giving the error which following pop dialog

  "The following program could not be installed.
  microsoft SQL server2005 Express edition set up cannot complete the installation
  -1"
 can any body help me


First of all, there is not operating system Windows 7XP. Other thing, we need more info. Is it fresh install ? Maybe you have other version of SQL installed ? What other software do you have in your PC ? Also you can read this What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?


Oh! sorry for wrong typed "Widows 7Xp" ie windows7.
thank you very much for the reply i chek it & update the feedback

regards
Algudkar sh..

Top
  7/8/2012, 8:34 AM
Joined 7/25/2009
Last visit: 5/23/2013
Posts: 409
Rating:
Rated: Very Good [1.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Darius wrote:
algudkar wrote:
Hi experts and friends
now in my pc having windows 7xp os
iam going to install wincc flexible 2008 but it giving the error which following pop dialog

  "The following program could not be installed.
  microsoft SQL server2005 Express edition set up cannot complete the installation
  -1"
 can any body help me


First of all, there is not operating system Windows 7XP. Other thing, we need more info. Is it fresh install ? Maybe you have other version of SQL installed ? What other software do you have in your PC ? Also you can read this What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?


Hi darius
what you suggest above the link was i followed and also i formatted now windows XP sp2. now also iam facing the same problem also see the attached file

Attachment: error.zip  (15 Downloads)

regards
Algudkar sh..


Top
  7/10/2012, 4:49 PM
Joined 9/5/2011
Last visit: 5/23/2013
Posts: 2587
Rating:
Rated: Outstanding [3.83 out of 5 / rated 132 time(s)]. (132) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

you should do the point 1.4 in the following FAQ.

What are the possible causes of an unsuccessful Microsoft SQL Server 2005 Express installation or why is creating or opening a WinCC flexible 2008 project aborted?

Tweety
Top
  7/12/2012, 11:45 AM
Joined 7/25/2009
Last visit: 5/23/2013
Posts: 409
Rating:
Rated: Very Good [1.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 


Hi Tweety
thanks  for the reply
as you suggested point 1.4 in the FAQ. this link same was darius also suggested. i was sollwed the same step by step even also not solved......!

regards
Algudkar sh..

Top
  7/12/2012, 12:50 PM
Joined 9/5/2011
Last visit: 5/23/2013
Posts: 2587
Rating:
Rated: Outstanding [3.83 out of 5 / rated 132 time(s)]. (132) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

Do you use the right operating system?
Do you use the rigth WinCC flexible version?

You should check the list on the end of the following FAQ.

With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?

Which version of WinCC flexible do you use?
Do you install from CD?

Tweety
Top
  7/14/2012, 11:21 AM
Joined 7/25/2009
Last visit: 5/23/2013
Posts: 409
Rating:
Rated: Very Good [1.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Tweety wrote:
Hello,

Do you use the right operating system?
Do you use the rigth WinCC flexible version?

You should check the list on the end of the following FAQ.

With what are SIMATIC WinCC flexible 2008, 2007, 2005 and 2004 compatible?

Which version of WinCC flexible do you use?
Do you install from CD?

Tweety


Hi darius / Tweety
thank you for reply for this topic and keep in touch. finally i got the result.
i was install the first seperatly MSQL 2005.and next i was install the software wincc flex2008. now working fine but inthere iam trying to install winccflex 2008 sp2.its asking  please upgrade U13.what
is that iand where can i down load that  software..?

regards
Algudkar sh..

Top
  7/16/2012, 12:36 PM
Joined 4/24/2006
Last visit: 5/22/2013
Posts: 4676
Rating:
Rated: Excellent [4.12 out of 5 / rated 428 time(s)]. (428) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello algudkar,

Perhaps it means Update 13 for WinCC flexible 2008 SP2. blush

You can download here: Update for WinCC flexible 2008 Service Pack 2

Best regards,

Wizard
Top
  8/29/2012, 11:31 PM
Joined 10/24/2011
Last visit: 8/31/2012
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi algudkar,

I am stuck in the same step you were at and cannot solve it. How did you make it? I am installing MS SQL 2005 first and got the error? After uninstall SQL, try to reinstall it, but always fail.

Any suggestion are really appreciated.

Best Regards,

Jerry
Top
12» Page 1 of 2 (14 items)
Actions