Technical Forum

MICROMASTER

HW timer used ?

Thread Starter: SieMuzzy   Started: 7/8/2012 7:33 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/8/2012, 7:33 PM
Joined 1/21/2011
Last visit: 4/21/2013
Posts: 47
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello All

 I have a problem so My micromaster 440 have connected a encoder modul and encoder but when  ı wanted to start driver, driver was stop. So I checked Parametre 403, I realized to change  Bit4 of Pr403 (0-->1)   the mean of condition is Hw timer used but I never belief what is it..

thanks
best regrads
Top
  7/14/2012, 7:01 PM
Joined 1/21/2011
Last visit: 4/21/2013
Posts: 47
Rating:
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi All

I had a problem about "Hw timer Used?" So Thanks all of them checking this message but  I don't understand what any modarators answerd this question anyway I have solved so Encoder connection incorrect, Encoder rotation and  the direction of the encoder for driver isnt same so I changed A and /A and both the encoders start  rotating  same direct 

best regards
Thanks
Top
Thank you for this post from:
Page 1 of 1 (2 items)
Actions