Technical Forum

PC-based Automation

WinAC RTX 2008 fully virtual

Thread Starter: Jure Petrovic   Started: 4/9/2012 10:14 AM   Replies: 11

« Previous thread Next thread »
12» Page 1 of 2 (12 items)
  4/9/2012, 10:14 AM
Joined 3/15/2012
Last visit: 3/25/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Has anyone managed to fully virtualize WinAC RTX 2008?

With ethernet communication interface. So that one could use that on a laptop,
without Intel 82541PI Ethernet controller?

Thank you
Top
  4/24/2012, 9:07 AM
Joined 1/26/2011
Last visit: 5/16/2013
Posts: 179
Rating:
Rated: Excellent [4.47 out of 5 / rated 53 time(s)]. (53) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Jure Petrovic wrote:
Has anyone managed to fully virtualize WinAC RTX 2008?

With ethernet communication interface. So that one could use that on a laptop,
without Intel 82541PI Ethernet controller?

Thank you


So what exactly do you want to have?
fully virtualize without any interfaces?
because what you wrote is a little bit confusing. you want to have the RTX fully virtualize but also want to have a ethernet communication interface? Rnf:lblSmileyTooltip_  think

regards bigfoot
Top
  4/24/2012, 9:26 AM
Joined 3/15/2012
Last visit: 3/25/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Yes. But as far as I see it now, this cannot be done.
It would be great, if WinAC RTX would support any
generic network card.

I don't mean this for production, but for simulation/testing purposes.



Top
  4/24/2012, 10:04 AM
Joined 1/26/2011
Last visit: 5/16/2013
Posts: 179
Rating:
Rated: Excellent [4.47 out of 5 / rated 53 time(s)]. (53) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Oh i think it is possible to have the WinAC fully virtualize.

If you install STEP7 and WinAC RTX on the same computer and set the PG/PC Interface to internal you can simulate or test your program. You only have to set the PG/PC interface to internal and set the Component Configuration correctly.

This is the way i am testing my self made programs in STEP7.

greeting bigfoot
Top
  5/9/2012, 7:23 PM
Joined 6/23/2008
Last visit: 5/18/2013
Posts: 362
Rating:
Rated: Excellent [4.29 out of 5 / rated 17 time(s)]. (17) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

I think it's not a question of support by WinAC for the virtual network card.
It's more a question of support by VM-Ware. VM-Ware would need to have a realtime driver for their virtual network card.
It's only what I think.
Regards,
mark
Top
  7/11/2012, 1:59 PM
Joined 1/31/2007
Last visit: 9/29/2012
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Actually there is a work around.
Siemens sells an application called "WinAC IP Driver V2" that gives you access to the TCP stack of windows from the WinAC RTX. The normal T-blocks can't be used, but some slightly modyfied ones comes with the package. Works fine, is a little bit tricky to setup since the blocks are not able to be used as multi-instances.



/søren
Top
Thank you for this post from:
  7/14/2012, 11:15 AM
Joined 3/15/2012
Last visit: 3/25/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Thank you all for answers. 

To make the testing environment as real as possible I bought that Intel Ethernet card. Actually this was pretty good solution, as this ethernet cards cost around €20-25, which is not too bad. 

The only problem is, I cannot use this on a laptop on the field - but ok - I do most of the test stuff in the office anyway. 

This package might be useful, however changing all T-blocks just for tests and then back might get annoying in a while. However, I might try it anyway :-)
Top
  8/23/2012, 9:23 AM
Joined 11/22/2009
Last visit: 5/16/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi Jure,
Could you please describe a little bit more your final solution to this? I'm really interested in having a solution based on WinAC RTX and virtual machines to test our control code in simulation.
Thanks in advance,

Top
  9/14/2012, 11:17 PM
Joined 11/22/2009
Last visit: 5/16/2013
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Could you please let us know your current implementation? It would be very useful for all of us.
Thanks

Jure Petrovic wrote:
Thank you all for answers. 

To make the testing environment as real as possible I bought that Intel Ethernet card. Actually this was pretty good solution, as this ethernet cards cost around €20-25, which is not too bad. 

The only problem is, I cannot use this on a laptop on the field - but ok - I do most of the test stuff in the office anyway. 

This package might be useful, however changing all T-blocks just for tests and then back might get annoying in a while. However, I might try it anyway :-)
Top
  9/17/2012, 9:22 PM
Joined 3/15/2012
Last visit: 3/25/2013
Posts: 9
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Quike, 

I didn't virtualize it in the end. I am using WinAC natively on one PC with a supported Intel ethernet card. We use it only to test profinet communication with different devices. Regarding the price of the WinAC license, the intel ethernet card is for free!

Anything else can be pretty much tested in PLCSIM. 

If you really need it virtual, I would try that proposition above with IP driver v2. However, I am not sure if the profinet communication will work this way...

Rgds,
Jure 
Top
12» Page 1 of 2 (12 items)
Actions