The harddrive of the configured machine is died. now I replace the harddrive and tried configure by myself, but I got "hresult error 0x8004610a". I have been searching alot and still can't solve the problem.
I just want to make sure if something I'm missing.
the situation is below:
- Windows 2000 nt sp3
-wincc 6.0 sp3
-sql server 2000 sp3
-window administrador user with enough privilege, has password.
-already change auth to mixed mode
-I'm not sure if server and client can be the same computer. because it's not in LAN it's ip is 169.250.0.0 (strange ip)
- simatic shell shows the own computer
I neither can open existed projects nor create any new project (hresult error 0x8004610a)
any other suggestion?