Thread Starter: Victor Tech Started: 5/3/2012 11:47 PM Replies: 9
I am having a problem trying to transfer an existing project to a new MP277 10" touch with USB. the WinCC Flex is a new installation on Windows 7. The project had previously been maintained using WinCC Flexible 2005, and the panel was a MP270 10" touch. When trying to transfer I get a message "There are no devices selected for transfer. Select at least one device in the transfer dialog". There is nothing to select in the transfer dialog. Communication has been proven as i updated the OS on the panel using the USB master to master cable. Any ideas?