Technical Forum

PC-based Automation

How to manage communication between Sentron PAC 3200 and WinLC RTX

Thread Starter: JJLAMOROSO   Started: 2/15/2012 12:14 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  2/15/2012, 12:14 PM
Joined 1/25/2012
Last visit: 3/21/2013
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello

We currently try to establish a communication between a Sentron PAC 3200 and the WinLC RTX system via the ModbusTCP channel. (not via DP!).
we tried to use the T_CON/T_DISCON/T_SEND/T_RCV blocks with no success until now.
Is someone can give us informations or an example of configuration to set up this feature??

Thanks

 
Top
  2/15/2012, 2:25 PM
Joined 1/26/2011
Last visit: 5/21/2013
Posts: 179
Rating:
Rated: Excellent [4.47 out of 5 / rated 53 time(s)]. (53) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

for Modbus TCP connection there is a Wizard (Mobus TCP Wizard) available (with documentation).

http://support.automation.siemens.com/WW/view/en/31535566

I hope this can help you.

best regards bigfoot
Top
Page 1 of 1 (2 items)
Actions