Technical Forum

SIMATIC Addons / IT4Industry

When I try to select targetsystem S7-4k for FuzzyControl++ v5.0, it remains Not connected.

Thread Starter: Teu   Started: 6/2/2011 12:43 PM   Replies: 5

« Previous thread Next thread »
Page 1 of 1 (6 items)
  6/2/2011, 12:43 PM
Joined 5/25/2011
Last visit: 6/27/2011
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello!

I'm using the following software:
                 FuzzyControl++ v5.0
                 Step7 v5.4 Professional
                 Simatic NET 6.4
I'm trying to control a process using a fuzzy control. I made the project in step 7 containing FB30 and DB30, I download it to the PLC S7-300 and then I open the FuzzyControl++ 5.0 software. I select from the menu Targetsystem->Select->S7-4K and after I press OK status remains Not Connected. If I leave it so and select Targetsystem->Connect I receive the following error Target_S7_FZ "While checking an authorisation, error 0 in call to function 0 occured" and the "Connect" window is blocked. I can only press Cancel or Help.

What could I do? Someone could help me?

Thanks.
Top
  6/3/2011, 8:24 AM
Joined 10/3/2008
Last visit: 5/2/2013
Posts: 522
Rating:
Rated: Outstanding [3.46 out of 5 / rated 52 time(s)]. (52) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,
attach your S7 program and 2 screenshots of the connection dialog (with the entered values) and the error message.

Wüstenräuber
Top
  6/6/2011, 4:21 PM
Joined 5/25/2011
Last visit: 6/27/2011
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I've attached the following:
 - screenshots of the program made in s7 and sent to the plcsim (the s7-300 was unavailable for me a few days) ob1-1 -> ob1-5
 - screenshot of the pc-pg interface
 - screenshots of errors in fuzzycontrol++ 5.0 for targetsystem selection, connect

Attachment: fuzzycontrol++.zip  (30 Downloads)

Top
  6/7/2011, 1:59 PM
Joined 5/25/2011
Last visit: 6/27/2011
Posts: 3
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Anyone? Help please!
Top
  6/7/2011, 10:49 PM
Joined 10/3/2008
Last visit: 5/2/2013
Posts: 522
Rating:
Rated: Outstanding [3.46 out of 5 / rated 52 time(s)]. (52) 
Users with special expertise supervising conferences
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hi,
the parameters for the MPI connection are not valid. You have to set "Target address", "Rack" and "Slot" to valid values (have a look at the hardware config).

Do you have a valid fuzzy license in your ALM?

Wüstenräuber
Top
  6/9/2011, 8:34 AM
Joined 10/6/2008
Last visit: 1/10/2012
Posts: 8
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello Teu,

did you transfer the license to your computer?
The error message you got in "Target_S7_FZ" dialog means the license couldn't be found.
If you already transfered the license and it isn't recognized by the program you should contact IT4Industry Hotline.

Regards
Top
Page 1 of 1 (6 items)
Actions