Technical Forum

Other Process Control Systems

Trend Manager Braumat V5.3 + SP1 + HF3

Thread Starter: cocouv3   Started: 1/29/2010 4:26 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  1/29/2010, 4:26 PM
Joined 6/16/2008
Last visit: 4/24/2012
Posts: 1
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
I have a problem, whit some trend curves in Braumat V5.3, my configuration is  IOS01, IOS2 Redundant Servers and IOS12,IOS11,IOS21, Clients and 4 PCU
I have a license for trend Manager, and i have a big problem.

Some batch archive, i can see all the process value and in other i can not see all, only see a few process value, all the process value are taken from the braumat block "MESS", analogic input, I cant see it in the screen and in the variable table in step 7, But it is not showing in the trend picture. In some batches i cant see it at all in other not, I dont know why, it is aleatory
I revised the call in all the PCUs the call to the block FC695 "TRIGG_CURVE_GR_FC" and the input parameter "iID"  it have diferents group numbers in the 4 PCUs
I revised the "trending definition" and the process value are Ok, the Curve Group it is the same with the PCU and the Archive tag is Batch Archive
I revised the Trending Curve Input and the tags are the same that in the trending definition
I revised the trenman.ini and Kurven.ini and it is Ok,
The problem starts in November 2009 missing trending was 10%  in this 2010 the problem get worst the missing trend is like a 70% of the batches doing in the day

I will wait for some answer thanks a lot

Top
  7/20/2010, 4:12 PM
Joined 11/14/2009
Last visit: 7/20/2010
Posts: 5
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Do you still need help with this issue?  I may be able to help...

--------------------------------------------------------
Don't find fault, find a remedy.

Sparkblender
Top
Page 1 of 1 (2 items)
Actions