Other Process Control Systems
Cross-Coupling between Braumat CPU 416-4 and CPU 315-2PN/DP via Ethernet
Thread Starter: Pornprasert Started: 5/4/2009 7:03 AM Replies: 0

5/4/2009, 7:03 AM
|
Joined 11/21/2007
Last visit: 7/28/2009
Posts: 8
Rating:
(0)
|
(0)
|
Dear all,
I want to make a communication between Bramat V5.3 SP1, CPU416-4 and S7-300 CPU 315-2PN/DP via Ethernet (S7 Connection on TCP/IP). I have using BSEND/BRECV function block in CPU 315-2PN/DP and try to configure XC_CPU_32 and XC_JOB_32 in Braumat Parametrization. PCU_State/PCU_State_Conn_1/PCU_State_Conn_2 in XC_CPU_32 show error -1. But connection status in Netpro show connected. Status in XC_JOB_32 look like normal.
I tested to programming by myself in CPU 416-4 by call SFBs BSEND/BRECV in FB1220, it working normally
I have using PCU No. 31 for S7-300 CPU (Connection local ID = 1F) and Bramat PCU No. is PCU 2. Can I make a communication like this? What is the solution for this requirement?
Best regards,
Pornprasert.
|
|
|
|
Actions