Technical Forum

SIMATIC TDC, FM458, T400

TDC MEssage problem in WINCC

Thread Starter: himanshu   Started: 4/4/2012 4:04 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  4/4/2012, 4:04 PM
Joined 7/22/2009
Last visit: 5/15/2013
Posts: 20
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi...
I Have merged two CPU prorams in one CPU. The problem I am facing problem with message number/ID in CFC block. In some block  message numbers are generated and also messages are displayed on trigering but in some block neither message ID are generated nor it is displayed. I am using TDC transfer for it. 
Please help in this regard.
Top
  4/4/2012, 6:15 PM
Joined 8/25/2006
Last visit: 5/21/2013
Posts: 898
Rating:
Rated: Excellent [4.2 out of 5 / rated 85 time(s)]. (85) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello.
Could you please upload your program to understand better your problem.
What was before merging two programs into one?
When you merge programs did you make any modification in PMC function blocks configuration?
Have a look at example project about connection TDC-WinCC (it is installed with D7-SYS installation in sample projects -  'D7-TDC-WINCC').
Top
  5/24/2012, 7:14 AM
Joined 5/21/2012
Last visit: 5/26/2012
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
i think u have to compile and download your wincc server..because in ur CFC program, message number change after TDC  transfer due to new block added..so u have to update this message number in wincc server.
Top
Page 1 of 1 (3 items)
Actions