Hi Guys,
Good day!
I'm back again. This time I'm working with an Simatic 545. This is completely my first time working with 545.
The client wants to communicate it with Wonderware SCADA via Ethernet. I already found the Kepware driver to make them talk to each other. The PLC already has one ethernet module installed. I haven't seen it except on pictures. My questions are:
1. Can the 545 PLC accept two ethernet modules? specificaly, 2572-A?
2. If the answer to question 1 is a NO, can the 545 existing ethernet handle two SCADA communication? because right now it is already connected to a Local LAN and the client wants to have a SCADA in a remote station. They'll be using AT&T as sevice provider.
3. Is 2572-A compatible with Simatic 545 series?
4. I have TIsoft version 7 and working on it now. If the loaded program was configured using softshop, can I upload it using TIsoft?
Thank you very much. Hope some experts answer my questions.
Regards,
ry_fern