Technical Forum

Process Control Systems SIMATIC PCS 7

PCS7 v 7.1 - Alarm Messages - Using "Free1,Free2,Free3,Free4,Free5 Fields

Thread Starter: lamgar   Started: 3/23/2010 2:52 PM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  3/23/2010, 2:52 PM
Joined 7/29/2008
Last visit: 10/1/2010
Posts: 10
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
have a cross platform system with apacs/quadlog and PCS7 - we have graphics that are in a common area with alarms that belong to separate plants we need a user configurable field in the database to assign a plant name so the alarms can be sorted by plant for operations.

when tried these "Free#" fields in the user test blocks section of the alarm logging utility get over written by a full compile in  PCS7 and the DBA in APACS.

why are they there if you can't use them?


Top
  8/10/2012, 1:46 PM
Joined 11/4/2011
Last visit: 5/22/2013
Posts: 155
Rating:
Rated: Excellent [4.53 out of 5 / rated 19 time(s)]. (19) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
So what is the answer? How to use FreeX fields in PCS7?
I don't see them in a PCS7 Message Configuration window in CFC
Top
Page 1 of 1 (2 items)
Actions