Technical Forum

SINAMICS

Sinamics Terminal Control

Thread Starter: DeanZ   Started: 7/30/2012 6:51 AM   Replies: 4

« Previous thread Next thread »
Page 1 of 1 (5 items)
  7/30/2012, 6:51 AM
Joined 7/18/2012
Last visit: 5/14/2013
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello all,
- I have a problem with sinamics G120 PM240 CU240B-2. I'm new in using sinamics. My problem is I cannot run the PM using terminal control 9 and 5. I already set the following parameters:
P700 = 2, P0015 = 12, P840 = 722.0. I'm familiar with MM4, for MM4 just make sure that P700 = 2 and P701 = 1(ON/OFF), but there is no parameter P701 in sinamics. What is parameters is related with DIN?
And also I cannot online the drive using STARTER, the baud rate set is 9600. Anyone can help me please??blush...



=== Edited by DeanZ @ 8/2/2012 4:36 AM [GMT ] ===


Top
  7/31/2012, 2:03 PM
Joined 9/7/2010
Last visit: 5/17/2013
Posts: 165
Rating:
Rated: Excellent [4.86 out of 5 / rated 29 time(s)]. (29) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
for online issue just try to go online with starter by config PG/PC interface
And try to diagnose the DI0, which have to be green when you give ON command to drive..

U can Give ON command to drive with commisioning-> control pannel...

Regard
Deep Bhatt

"The art of being wise is knowing what to overlook"
Top
  8/2/2012, 4:46 AM
Joined 7/18/2012
Last visit: 5/14/2013
Posts: 15
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,

For online with starter I already set the PG/PC as following:
-COM 2
-9600(baud rate)
-And also I running by control panel.
-For micromaster 4 I have no problem online with starter, but problem comes when I use sinamics.When I click accesible nodes - no devices found.
Top
  8/3/2012, 11:54 AM
Joined 12/16/2011
Last visit: 4/29/2013
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 

 

 

Dear Deanz,

             First of all check whether the cable is in working condition.Then you check whether you selected the exact drive unit. If both of this are correct, then you go for accessible nodes

If you are operating through terminals, then you please go for control drawing for digital input, which is given at the end of the manual.


 

 

 

Top
  8/4/2012, 2:18 PM
Joined 9/7/2010
Last visit: 5/17/2013
Posts: 165
Rating:
Rated: Excellent [4.86 out of 5 / rated 29 time(s)]. (29) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
DeanZ schrieb:
Hello all,
- I have a problem with sinamics G120 PM240 CU240B-2. I'm new in using sinamics. My problem is I cannot run the PM using terminal control 9 and 5. I already set the following parameters:
P700 = 2, P0015 = 12, P840 = 722.0. I'm familiar with MM4, for MM4 just make sure that P700 = 2 and P701 = 1(ON/OFF), but there is no parameter P701 in sinamics. What is parameters is related with DIN?
And also I cannot online the drive using STARTER, the baud rate set is 9600. Anyone can help me please??blush...



have u checked p2010 and p2011 ?? it have to be same as u have configured in PG/PC interface setting..

Regard
Deep Bhatt

"The art of being wise is knowing what to overlook"
Top
Page 1 of 1 (5 items)
Actions