Technical Forum

Decentral Peripherie

Problem with

Thread Starter: norman paul   Started: 7/20/2012 4:17 AM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  7/20/2012, 4:17 AM
Joined 5/14/2012
Last visit: 4/1/2013
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Good day,

Recently, i have encountered this problem regarding IM151-7 module, first is the personel in-charge reported it busted (burnt) in which the reason is still not clarified (currently under investigation), though im still a bit puzzled because there are output in the modules attached. though i couldn't communicate with the module itself (which i think is the busted part), to confirm, ive tried to connect to another IM 151-7 module and yes, i connected..

the second problem arises, though i connected with it, the module indicates a [?] and tells that it needs a master module. so i really couldn't see whats inside of it. the personel said that there is no master module existed and only relies on the memory card inserted, so im assuming that the original programmer didn't want others to connect to it though.

how would i be able to check on the other i/o modules if they are also damaged if i ont have a master module?

Attachment: photo.JPG  (7 Downloads)

Top
  7/20/2012, 6:35 AM
Joined 2/22/2011
Last visit: 5/18/2013
Posts: 90
Rating:
Rated: Excellent [4.5 out of 5 / rated 2 time(s)]. (2) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
norman paul wrote:
Good day,

Recently, i have encountered this problem regarding IM151-7 module, first is the personel in-charge reported it busted (burnt) in which the reason is still not clarified (currently under investigation), though im still a bit puzzled because there are output in the modules attached. though i couldn't communicate with the module itself (which i think is the busted part), to confirm, ive tried to connect to another IM 151-7 module and yes, i connected..

the second problem arises, though i connected with it, the module indicates a [?] and tells that it needs a master module. so i really couldn't see whats inside of it. the personel said that there is no master module existed and only relies on the memory card inserted, so im assuming that the original programmer didn't want others to connect to it though.

how would i be able to check on the other i/o modules if they are also damaged if i ont have a master module?

  dear
     u can check in hardware of the program by getting online solve the problem by diagnose window ..

Thanks regards
ANBUGEETHAN GOWDA
Top
  7/23/2012, 3:20 AM
Joined 5/14/2012
Last visit: 4/1/2013
Posts: 6
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
hi,

can you tell me abit more of this online support. kinda confused. thanks grin
Top
  7/23/2012, 8:07 AM
Joined 3/21/2006
Last visit: 5/14/2013
Posts: 9063
Rating:
Rated: Outstanding [3.78 out of 5 / rated 820 time(s)]. (820) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
norman paul wrote:
hi,

can you tell me abit more of this online support. kinda confused. thanks grin

Top
Page 1 of 1 (4 items)
Actions