Technical Forum

Motion Control System SIMOTION

Mismatch in Simotion Programe.

Thread Starter: P.Singhania   Started: 7/16/2012 2:23 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  7/16/2012, 2:23 PM
Joined 6/14/2012
Last visit: 3/20/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear All,

I have a simotion programe D435 of which  the available latest backup dose not match in 1 ST program. Rest all axis, programs and drives are matching.

On comparing online, the source code of that ST prog shows mismatch and compilation result and HMI relevant data seems to be match. Also the used technology packages show mismatch.

Can anyone help me out on this??  Is there any way to find out where dose exactly the program is mismatch. It will be also convineant if I get the mismatch line no. of that ST prog.


Warm Regards,
Prasahnt Singhania
Top
  7/16/2012, 2:39 PM
Joined 5/12/2006
Last visit: 5/17/2013
Posts: 1546
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

with which version do you work?
Have you download the project to the D435 with the option "Store additional data on the target"?

You can test if the diffs where see with the "project comparsion" from the toolbar in Scout.

Regards
Christoph
Top
  7/17/2012, 7:34 AM
Joined 6/14/2012
Last visit: 3/20/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

I am using scout V4.2 and the project was done in V4.1. 

The option ' load additional data on target system ' was NOT tick.

I have also performed the online-offline comparison and the result shoes, Source code mismatch but compilation result and hmi relevant data shows match.

Is there any way to find the line no. where it is mismatch??

Warm Regards,
Prashant Singhania
Top
  7/17/2012, 11:46 AM
Joined 5/12/2006
Last visit: 5/17/2013
Posts: 1546
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

without the option no code data where stored in the target system so you can't get the code line which is mismatch.

Regards
Christoph
Top
Page 1 of 1 (4 items)
Actions