Technical Forum

SIMATIC WinCC flexible

MP277

Thread Starter: ashishm   Started: 7/14/2012 9:52 AM   Replies: 1

« Previous thread Next thread »
Page 1 of 1 (2 items)
  7/14/2012, 9:52 AM
Joined 2/1/2011
Last visit: 5/24/2013
Posts: 39
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Dear Sir,
I have MP277 8" Touch. In that i am logging data through data log option availaible in Wincc Flexible. through script excel file from MMC storage card is copied to USB. Problem is that when we open that file than all fields are in single field and is not in proper format. finally concluded that data is not logging properly in excel file that is store in MMC storage card. so is there any other setting to do for proper data log in MMC storage card through Wincc Flexible.
Top
  7/18/2012, 4:14 PM
Joined 9/5/2011
Last visit: 5/24/2013
Posts: 2595
Rating:
Rated: Outstanding [3.83 out of 5 / rated 132 time(s)]. (132) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

you can find more information about logging in the following links.

How are tags and alarms logged in WinCC flexible?

How do you do long-term archiving with WinCC flexible?

Tweety
Top
Page 1 of 1 (2 items)
Actions