Technical Forum

SINAMICS

S120 & G120 Drive Network Setup Help <

Thread Starter: RPM2012   Started: 7/5/2012 6:05 PM   Replies: 0

« Previous thread Next thread »
Page 1 of 1 (1 items)
  7/5/2012, 6:05 PM
Joined 6/4/2012
Last visit: 4/11/2013
Posts: 12
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
I need to put an S120 drive and G120 drive into a Profinet network but have not done this before so need some help. I got the S120's compact flash card and tried to insert the GSD but the file was already there. Then I tried to insert the universal S120 drive into hardware confgurator but it say it needed to go into PN-IO device but it just connects directly to the network switch. I'm a little confused on what I need to do to get the drives working on the network. Any help is appreciated.



=== Edited by RPM2012 @ 7/5/2012 6:06 PM [GMT ] ===


Top
Page 1 of 1 (1 items)
Actions