SINAMICS
DCC for angle synchronisation in S120
Thread Starter: DavidBrown Started: 6/29/2012 3:46 PM Replies: 1

6/29/2012, 3:46 PM
|
Joined 6/29/2012
Last visit: 6/15/2013
Posts: 69
Rating:
(0)
|
(0)
|
I thought there was a DCC-function available for angle synchronisation in S120, but I cannot find it anywhere? What is approximately the cpu-load the DCC takes?, how many axes may there be in the cpu, next to the two synchronised axes? Is there documentation available about the function?
|
|
|
|

7/1/2012, 8:18 PM
|
Joined 5/22/2012
Last visit: 6/15/2013
Posts: 111
Rating:
(9)
|
(0)
|
For angle sync you don`t need DCC. It`s possible with the basic positioner. You only have to use the same setpoints and start the movement at the same time (for example, use the same binector for the start signal). So you can have up to six axis on one CU320-2. Or do you need an external encoder ("real master")?
|
|
|
|
Actions