Technical Forum

Motion Control System SIMOTION

SU/PF Led continuoes YELLOW

Thread Starter: sparten   Started: 6/2/2012 1:29 PM   Replies: 3

« Previous thread Next thread »
Page 1 of 1 (4 items)
  6/2/2012, 1:29 PM
Joined 8/2/2011
Last visit: 5/21/2013
Posts: 96
Rating:
Rated: Outstanding [3.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi expert,
              i am using simotion cuD425 with version4.1 and scout version 4.2.1.0...i have successfuly downloade dmy project in cu but my cu comming in RUN mode ...on cu LED SU/PF is continuose YELLO also other LED status as follow:
RDY continuose GREEN,
RUN flashing Green ..
i have reffered in says that for this LED status "Transition from STOPU-RUn"..
.i am not able to execute my use programme...,,pls help me to get my cu in RUN condition
Top
  6/2/2012, 3:07 PM
Joined 5/12/2006
Last visit: 5/25/2013
Posts: 1552
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

check the diagnostic buffer of the CPU, you can post it here for anlyse.
Have you a program in the StartUP Task?

Regards
Christoph
Top
  6/4/2012, 6:31 AM
Joined 8/2/2011
Last visit: 5/21/2013
Posts: 96
Rating:
Rated: Outstanding [3.5 out of 5 / rated 4 time(s)]. (4) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hi,
    in dignostic buffer it shows me that there is transittion from STOPU to RUN mode..
i will send you dignostic buffer file soon ..
also i have configured same motion task in starup task....i will send you make project...
Top
  6/4/2012, 8:25 AM
Joined 5/12/2006
Last visit: 5/25/2013
Posts: 1552
Rating:
Rated: Excellent [4.18 out of 5 / rated 115 time(s)]. (115) 
Users with special expertise supervising conferences
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello,

what do you mean with " configured same motion task in starup task"?

Thats no good idea when you execute the code from a motion task in the startuptask.
Example:

enable Axis in startuptask dosn't work because the BZ RUN must reached to enable the axis!

Regards
Christoph
Top
Page 1 of 1 (4 items)
Actions