Technical Forum

LOGO!

manual control for digital output

Thread Starter: corneliu01   Started: 5/22/2012 7:13 PM   Replies: 2

« Previous thread Next thread »
Page 1 of 1 (3 items)
  5/22/2012, 7:13 PM
Joined 10/21/2011
Last visit: 5/31/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello!

 I try to do for this program controled by a sensor, a manual control using the entries i1 and i2
Auto Part I managed to do it.
We added noise filters possible.
I can not make a control manual, which override the sensor command.
I want to use two inputs (i1 and i2).
I1 to increase. For example, if the sensor value is 450, then clicking on i1, to increase the value gradually (not suddenly) up disable input i1.
After disabling i1, the value to remain in place.
Also for i2, only the value decreases.
Plus another input (I3) to switch between automatic or manual control.
for example, i3 = 0, then control is automatic,  for i3 = 1 then control is manual.


Please, help me
add and manual control.

Attachment: control sensor.zip  (35 Downloads)

Top
  5/30/2012, 8:29 PM
Joined 1/5/2007
Last visit: 5/16/2013
Posts: 1468
Rating:
Rated: Outstanding [3.98 out of 5 / rated 401 time(s)]. (401) 
Users with special expertise supervising conferences
Rated: Excellent [5 out of 5 / rated 1 time(s)]. (1) 
Hello,

plaese look at the attachmet to find my solution /answer tu you..

File "DEMO_control_sensor_with_auto_and_hand_control_V1 (0BA6).lsc" contains my part to demonstrate how it works.
                                                       blink
File "DEMO_control_sensor_with_auto_and_hand_control_V1x (0BA6).lsc" contains the combination of my solution with your circuit "control sensor.lsc"....

If you have questions ask me here...

Best regards
Betel

Attachment: FORUM_control_sensor_V1.zip  (32 Downloads)

Top
Thank you for this post from:
  5/31/2012, 9:25 PM
Joined 10/21/2011
Last visit: 5/31/2012
Posts: 2
Rating:
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Rated: no ratings [0 out of 5 / rated 0 time(s)]. (0) 
Hello!

I have no question.
And your example is very helpful.
Thank you very much.
Top
Thank you for this post from:
Page 1 of 1 (3 items)
Actions